MDU Footprint Tools

DHFC provides a set of tools to work with multiple dwelling units (MDUs). These tools help you sketch the basic schematics of the building to include floors and other structural elements, such as access rooms. Plus, you can add labels.

For stranding and the RF network, use the standard Place Strand tool and Place RF Network tool. There are not separate network sketch tools inside an MDU. For an example of an installation inside an MDU, see the topic MDU Workflow.

Tool

Description

Draw Footprint

This tool sketches a rectangular footprint of the MDU.

View Footprint

This tool “opens” an existing MDU footprint for further editing. View a footprint first to then sketch floors, sketch other structural elements, add labels, or use the Auto Create Strand tool.

Draw Lines

This tool adds line graphics to the inside of the MDU. It is not a stranding tool. Instead, it is used to add helpful sketch elements to the MDU, such as an access room location inside the building.

Draw Rectangle

This tool adds rectangle graphics to the inside of the MDU. Much like Draw Lines, it is used to add helpful sketch elements to the MDU, such as an access room location inside the building or a floor.

Draw Geometry

This tool adds polygon graphics to the inside of the MDU. Much like Draw Rectangle, it is used to add helpful sketch elements to the MDU, such as an access room location inside the building.

Draw Floors

This tool sketches evenly-spaced rectangles in bulk. For example, you could sketch 7 floors at once. It also supports horizontally-oriented sketching, which is helpful to sketch single-story duplexes or triplexes, for example.

Auto Create Strand

This tool places stranding in bulk. For example, it can place stranding for 7 floors at once.

Draw Text

This tool adds text to the inside of the MDU. It is helpful for labeling floors or adding other notes, such as the access room name or number.

Edit

This tool lets you edit existing sketch or text elements. It is helpful for correcting a previously-sketched shape or text.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.