Optimize Underground Structure Size

This tool optimizes the underground structure for all components that are downstream from the point where you clicked.

The following are the optimizations performed for each item:

  • Locates all components attached to a given underground structure

  • Sums all the components that have a point field on the spec

  • Searches the underground structure types defined in Designer HFC Catalog for the first one in which the component point sum falls between the min and max point values

TIP: If a perfect match isn't found, the first underground structure type whose max point value is greater than the component point sum is returned.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.