Move a Component

Available for These Components

Notes

All components

This action allows you to move a component to a different location on the map and to move a component a full 360°. Grid lines appear in the map, and movable components can be snapped to the grid lines. Hold down the Ctrl key to move components with more precision. When two or more components are connected, the components will be moved as a group.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.