Swap Plugins
Components such as conditioning taps and inline equalizers (LEQs) can be coupled with a variety of plugins. In the Component tab, you can swap out the plugins for conditioning taps and LEQs that are a part of your design. When swapping a plugin, keep the following points in mind:
-
The plugin section in the Component tab only appears for applicable components. If a normal tap is selected, for example, the plugin section and the Swap button are not available or visible.
-
Conditioning taps and inline equalizers (LEQs) can be configured to have a default plugin. If no default is configured, the component uses whatever plugin is listed first in the list of plugins. See the topic Plugins in the DHFC Configuration Guide.
-
Conditioning taps have one slot available for a plugin. The current plugin is displayed by the Swap button.
-
LEQs only use return attenuators for plugins.
-
Plugins are also annotated on the map next to the tap or equalizer symbol. See Plugin Annotations for more information.
-
The Swap functional is also available for amplifiers. See the topic Amplifier Plugins for more information.
Plugins are saved as a part of your design, just like any other component.
To swap a plugin, follow these steps: