How do I split a node when replacing an existing amp with a node?

  1. Right-click the component and replace it with a node.
  2. Reverse the signal on the leg that needs to have the signal reversed, assuming that is needed.
  3. Swap the legs around to conform to your design needs.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.