Draw Lines, Rectangle, Geometry

These draw tools allow you to add other sketch features inside the MDU. Commonly, they are used to add details about access rooms, conduit inside the building, and other features that might be helpful for an engineer to understand nuances of the MDU. These tools work similarly. To use them:
  1. First, use the View Footprint tool to see the inside of the MDU.
  2. Click either the Draw Lines tool, Draw Rectangle tool, or Draw Geometry tool. Notice your cursor changes into a crosshair.
  3. Sketch the shape inside the MDU. The sketch behavior depends on the tool:
    1. Draw Lines: Each click adds a vertex to the line. Press Esc to stop sketching the line.
    2. Draw Rectangle: Click and hold, then move your cursor. Upon releasing the cursor, the application draws the rectangle.
    3. Draw Geometry: Each click adds a vertex to the polygon. Double-click to finish the sketch.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.