Power Blocking - Node

Designer HFC allows for blocking power on one or more ports of a node.

Power Blocking

To block or unblock power to a port, toggle selection of the checkbox next to the port letter. When blocking power to a port of the node, the cartographic symbol for power blocking is displayed on the port and on the node port in the map.

If you block power to a port of the node then decide to unblock power to that port, you will need to reestablish connectivity to that port. Click the radio button next to the port to connect from, then click the radio button next to the port that you unblocked, to establish connectivity.

The following screenshot shows power blocking removed (the checkbox for the port is rechecked) from port D, though it has no connectivity:

To establish connectivity for port D, click the radio button:

Click the radio button of another port in the node and connectivity is established to the unblocked port:

Powering Port

One port on the node must be designated as the powering port. After placing a node, the default powering port is A, as denoted by the blue, right-facing pointer icon.

To change the powering port, select a different port from the drop-down list.

After you select a port from the drop-down list, the right-facing pointer situates itself next to that port in the Power Blocking diagram.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.