Leg Label Adjustment

Use this tool to adjust leg labels on nodes, which gives you the ability to change the letter labels, A through D, on the ports of the node.

Adjust a Leg Label

  1. Select a node then click the Adjust Leg Label  icon.
  2. Click a port letter to activate the port selector  icon.
  3. Click the port letter that you want to switch with another port. A grey port selector icon appears on the port.
  4. Click another port letter to perform the adjustment. You will see the two port letters switch places.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.