Swap a Component

Available for These Components

Notes

Amplifier

Directional Coupler

Power Supply

Splitter

Click to swap the output port of a component to a different port.

Node

When swapping a node that does not have a power-only port with a node that does have a power-only port, it is assumed that the node is powered through the power-only port.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.