How do I add a Do Not Build boundary?

Follow these steps to add a Do Not Build boundary to your design:

  1. Click the Draw Do Not Build Boundary  icon. The map cursor becomes a crosshair.
  2. Click in the map where you want to start drawing the boundary.
  3. Subsequent clicks in the map will add points to the polygon that define the boundary.
  4. Double-click the map to complete drawing the boundary. Thick, pale-taupe dashes create the perimeter of the boundary.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.