Jump Power

Power inserters are used when you need to jump power from one node or design location to another.

If applicable, search for and import the node from which you want to jump power. In this example, a node called SE14 has been imported into the design.

The imported node is highlighted in the map as well.

Power needs jumped between the proposed network on the left and the as-built, imported node boundary on the right.

Insert a power inserter on the terminated tap at the top of the proposed network on the left.

Click the Place RF Network  icon, select the power inserter you just inserted, then click the power inserter on the tap in the node boundary. Power is jumped between the two networks.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.