Draw Text

This tool adds text labels to the MDU. It is commonly used to add floor numbers and other descriptive elements to the MDU diagram. To use this tool:
  1. First, use the View Footprint tool to see the inside of the MDU.
  2. Click the Draw Text tool. Notice your cursor changes to a crosshair.
  3. Click inside the MDU, and a text prompt appears.

  4. Type your label, then click OK.
  5. Repeat as necessary to add labels to the MDU.

    TIP: To update the text, use the Edit tool. You can change the text itself, and you can also drag the text into a new position. To delete the text entirely, delete the words and click OK.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.