Lock All and Unlock All

When you have multiple components selected on the map, you can Lock All or Unlock All.

TIP: You can multi-select components with either the Marquee Select tool or holding Ctrl and using the Inspect tool.

Locked components are not automatically optimized. Additionally, any locked components that are uploaded to GIS will be retained as locked when the design is re-opened.

In the Component tab, the availability of the Lock All and Unlock All buttons depends on what is selected:

  • If only unlocked components are selected, then only Lock All is available.

  • If only locked components are selected, then only Unlock All is available.

  • If a mix of locked and unlocked components are available, then both Lock All and Unlock All are available.

TIP: You can also find Lock All and Unlock All on the right-click context wheel. Just like the Component tab, the availability of the buttons depends on what is selected. In the following image, both locked and unlocked components are selected, and thus, both Lock All and Unlock All are available on the context wheel.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.