Component Multi-Select

DHFC provides the ability to change the spec and/or behavior of multiple components via the Context Wheel.

When you hold down Ctrl and select multiple components in the map, you can right-click on any component to view the available Context Wheel options.

In the image below, two cables in the network are selected, and the available right-click option is Spec.

TIP: When you multi-select two or more taps, the only available option is Remove.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.