Reverse Signal

When you select this tool and hover over a component, a connectivity trace is initiated on each component. If the trace doesn't result in a node, then it will be highlighted, and the signal can be reversed.

If you reverse the signal on a directional coupler, then the component whose signal you are reversing is moved to the input.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.