Basemaps Tab

The Basemaps view provides various basemaps that you can click to view as the background of your map. The available basemaps are set by your administrator.

Custom basemaps added by your administrator will not include a detailed thumbnail image like the ones available for default basemaps. Long basemap names have a tool tip associated with them that displays the entire custom basemap name.

You can identify a custom basemap by the following thumbnail example:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.