Amplifier Plugins

Designer HFC provides the ability to configure and select/swap amplifier internals.

Click an amplifier in the map and on the Component tab, scroll down to view plugin information.

A Swap  button is available for internals that can be swapped in the amplifier. Click the button to view a dialogue of available plugins for swapping.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.