Publish Design

Use the Publish Design  tool to save a design to GIS for viewing by other people in your organization.

IMPORTANT:
  • You can control whether or not a confirmation prompt appears if your design is about to overwrite nodes in the GIS. See Settings for more information.

  • As it states in Settings, if you check both prompt options, you are only notified if the publish action is going to affect adjacent or non-design nodes. If that is not desired, cancel the publish. Then, import those adjacent, non-design nodes, resolve any conflicts, and publish again as a complete set.

This tool saves design data in a status of proposed. This tool does not commission the design, which saves the design data in as-built tables.

If you want to commit the design, use the Publish As Built  tool.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.