Spec a Component or Structure

Available for These Components

Notes

All Components

This action allows you to change the specification for the component. Click to select a different specification for the same type of component. This behavior differs from the action of Replace, which allows you to change the selected component to a similar one or to a completely different component.

Structures

Overhead and underground structures are optimized upon placement in the map. This action allows you to change the specification of the structure.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.