Default Components

Component defaults can be set up in DHFC Catalog, and those defaults display on the DHFC Catalog  tab, which you can view by selecting a component category from the drop-down list.

TIP: Setting default component values in DHFC Catalog is not required, so you may not see components denoted with Default in DHFC.

If you click on the radio button for a different component in the list, that component will be the default when placed within the network.

IMPORTANT: Changing the component that is placed by default in DHFC does not change the default value set in DHFC Catalog.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.