Place RF Network

Use the place RF Network tool to place network components in your design.

TIP: You can quickly build a simple RF network by clicking a strand point to place a node, then clicking the point at the end of the network. Designer HFC will automatically place taps at all points between the node and the last tap. Calculations for tap selection are based on the forward and return signal levels.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.