Attribute Editor
The Component tab includes an Attribute Editor. For example, the following image shows an example of editable attributes for a pole:
The fields available to edit vary by component type and by customer, and depending on your configuration, some components do not have any editable fields. Thus, the fields you see on your application might differ from the image above.
-
In Attribute Editor, some system fields are explicitly hidden from users. These are typically fields that appear elsewhere in the interface or do not provide useful information to users.
For example, the InternalPowerMapping field has values, but they are presented to users as an operable diagram, which is far more useful than the raw value itself. There is no attribute setting in the schema.xml to change the hidden nature of these fields.
-
In string fields, angle brackets < > are not supported and result in errors when pushing a design back to the GIS.
-
We recommend you enable web content filtering in ArcGIS Server.
After editing fields, click Save. This saves the changes to the fields, but it does not save the entire project. To have your changes persist beyond the current session, always save the entire project.
Cable Lengths and Strand Lengths
As described in the topic Cable Lengths, there is a relationship between the cable length and the strand length(s). In short, a cable’s length is driven by the span length (and by structures and transitions, if present), and in a multiple-span installation, the cable length is driven by the sum of those spans.
If you edit a span length using the Attribute Editor, the cable length is automatically adjusted. For example, if the installation has three spans with measurements of 100 feet, 200 feet, and 300 feet, the cable length would be 600 feet. If you later update the second span from 200 feet to 225 feet, the cable length automatically adjusts to be 625 feet.