How do I move a node from one location to another once a design is complete?

DHFC does not allow a node, nor any component, to move from one structure to another. You must either delete the component and place a new one, or delete one and replace another component with the desired one. You can, however, change the structure in ArcMap using the Aerial/UndergroundStructureId fields.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.