Power One-line Diagram

In addition to the signal one-line diagram, as you design your network, DHFC creates a power one-line diagram of the current port leg in the one-line viewport toward the bottom of the HUD.

 

If the network is powered, the one-line diagram displays the current RF leg and all its components. DHFC displays the physical distance between components by labeling the line connecting the icons with the relevant footage. You can click on an icon to have the data for that component display in the left column and to highlight the component's icon on the map.

Refer to the Map Symbols topic to understand symbols that display in the one-line diagram.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.