What types of stranding operations can be performed in DHFC versus ArcMap?

ArcMap can handle all stranding operations, assuming that NetworkIDs are properly assigned.

DHFC can help you:

  • Place address points including MDU address points

  • Adjust house counts {excluding vacant counts}

  • Place overhead and underground structures

  • Place a lockbox

  • Place demarcation points and MDU footprints

  • Place a vertex in an underground strand

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.