Insert a Component

Available for These Components

Notes

Amplifier

Directional Coupler

In Line Equalizer Reverse Conditioner (LEQ/RC)

Power Inserter

Splice

Splitter

Tap

  • Conditioning Tap

After you click Insert, the application waits for you to choose the appropriate upstream or downstream triangle. After choosing the appropriate triangle, find the component from the Insert Component menu. Double-click a component, and the component is placed.

Node

Click a port on the node to select placement of the component. Double-click a component in the Insert Component menu, and the component is placed on the node at the port you selected.

Power Supply

Terminator

For these two components, the Insert only works downstream. Thus, the application does not wait for you to choose the appropriate upstream or downstream triangle. It automatically uses the downstream triangle. Double-click a component in the Insert Component menu, and the component will be placed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.