Inspect Hotkeys

With the Inspect tool active, these hotkeys help to manipulate components placed in the map.

Action

Key

Adjust length (pertains to MDUs)

L

Allow the auto-optimize engine to optimize component

O

Change the specification of a component

C

Complete drawing of boundary

Enter

Delete a component

Delete

Display a Set House Count text box

H

Flip or swap ports

X

Multi-select components

Ctrl

Rename component

N

Replace component

R

Swap the target port during Arrange

Tab

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.