Rename a Component

Available for These Components

Notes

All components

This action allows you to change the component's name. Most component names are set in the DHFC Catalog. For nodes and power supplies, the names are typed with the components are added to the design.

You can also change the name in the Component pane, as seen in the video below.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.