Signal Information

The information provided depends upon the type of component selected. For example, a 4-port node has signal information for outputs A through D; an amplifier has signal information for input, output 1, and output 2.

Additionally, signal information can be viewed in either discrete  form or graph  form. If you switch from discrete to graph, that change is persisted when you click on another component.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.