Replace a Component

Available for These Components

Notes

All components

Click a component from the list to replace the current one. This action allows you to change the current component to a similar one or to a completely different component altogether. Having said that, if you are looking to change the spec associated with the current component but leave the component type alone, the Spec function is better suited to that workflow.

TIP: Internal components cannot be replaced on a point or line component.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.