Edit

The Edit tool allows you to modify existing graphics and text inside the MDU.

For example, click an existing text block to change the label. You can also drag and drop the text into a desired position using the “handle” on the left-hand side of the Text dialog.

When you click a shape, the vertices of that shape appear. Drag them into a desired position, or use the dark blue square to rotate the entire shape. Press Enter to accept the changes.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.