Select Alternate Routes/Paths

Previously when placing cable along a stranding network with parallel alternate paths, it was difficult to determine which path would be chosen when you clicked because the paths are close together and the path was automatically selected.

You want to select a path that is extremely close to another parallel path:

 

But which path will be used?

The following steps show the ease of selecting parallel paths:

  1. Zoom in and click to select the inner path, which becomes highlighted.

  2. Click the target and the cable is placed.
  3. Place another cable by selecting the outer path.

  4. Verify that each cable is associated with the proper stranding.

  5. Notice that this works with crossed paths as well.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.