One-line Map

The one-line map view is positioned below the strand map in the Designer HFC user interface, which allows you to view design details without leaving the strand map view. The HUD displays either the signal diagram for the current RF network leg or the power diagram. You can toggle between the signal view and power view using the buttons on the left of the one-line map.

TIP: Right-click and select Float to undock the one-line map from the strand map. This action floats all project tabs and the signal/power one-line diagrams in one grouping.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.