Power Blocking - Amplifier

Designer HFC allows for blocking power on the input port or the output ports of an amplifier.

Power Blocking

To block or unblock power to a port, toggle selection of the checkbox next to the port name or number. When blocking power to a port, the cartographic symbol for power blocking is displayed on the port (and on the amplifier in the map).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.