Flip a Component

Available for These Components

Notes

Amplifier

Directional Coupler

Power Inserter

Power Supply

Splitter

This action is available when two or more components are adjacent to each other in a top to bottom or side to side arrangement. Once you click Flip, the application automatically flips the orientation of the components.

If you need to specify a different port or side instead of the opposite port or side, use Arrange instead.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.