Remove a Component

Available for These Components

Notes

All components

  • This action allows you to remove a component from the design and the map.

  • You can only remove components that are part of your design. You cannot remove components that have already been pushed to the GIS and given an Esri Object ID.

  • You can remove multiple RF components at the same time, and you can remove multiple stranding components at the same time. But, because the multi-select options do not allow you to select from both the RF and stranding networks, you cannot perform the remove action against the two networks at the same time.

  • When you remove stranding components, the application automatically removes the associated RF components.

  • If the remove option is unavailable, it is most likely because a component with an Object ID is selected or is part of a multi-selection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.