Hotdots

Hotdots display on amplifiers  and splitters , and they represent the port on the component that is sending the strongest signal.

This information is also represented in the left portion of the HUD, underneath Signal Information. The following image shows a dot denoting the port that sends the strongest signal:

TIP: A hotdot does not display on an amplifier with a jumper plugin.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.