GPS and Windows Location Services

Designer XI has GPS capabilities to display the device’s location on the map. The application exclusively uses Windows Location Services for this functionality. At your company, your field crew might already have GPS devices that they routinely use. In order for Designer XI to consume the GPS data from the device, you need an intermediary such as GPSDirect to connect the device’s output to Windows Location Services, which then feeds the information to Designer XI.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?