Install the Designer XI Client Application

Install the application to validate the implementation and continue the configurations that occur within the client application. The installers can be downloaded via Solution Center > Rollout > ArcFM Designer XI. See the topic Rollout for more information (in particular, scroll down to the sub-header “Copy Download Link”).

Take it for a drive! (The link opens the Solution Center app and accesses the Rollout plugin.)

Although the Designer XI client application only requires the .NET framework to run, other applications are needed for a fully functional implementation.

Ensure the required applications are at a supported version and license level. For the most up-to-date information about supported versions and licenses, visit the myArcFM page Supported Versions and License Levels — Designer XI Client and Services.

  • For Geometric Network (GN) implementations, the following applications are required:

    • ArcGIS Server

    • ArcGIS Desktop

    • ArcGIS Runtime

    • ArcFM Server

    • ArcFM Desktop

    • ArcFM Solution Center

  • For Utility Network (UN) implementations, the following applications are required:

IMPORTANT: For GN implementations, ArcFM Server and Desktop are required because Designer XI leverages their reconciliation and post processes. Further, Designer XI uses model names and autoupdaters, much like any ArcFM implementation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.