Create and Publish Offline Tile Package Basemaps

While offline, Designer XI uses tile packages for basemaps (backdrops). Designer XI supports both vector (.vtpk) and raster (.tpk) tile packages for basemaps. Raster tile packages are created in ArcMap and saved as a .tpk file, and vector tile packages are created in ArcGIS Pro and saved as a .vtpk file. Then, the files are uploaded in Solution Center > Designer > Mapping > Tile Packages and downloaded to the clients for consumption by Designer XI.

IMPORTANT: All backdrops (including tile packages) must use the same projection that is defined in the electric or gas network..

For performance considerations, Schneider Electric strongly recommends vector tile packages (.vtpk) instead of raster tile packages (.tpk).

  • While online, the application automatically uses the .vtpk first if it exists. This offers better performance than an online map service. If a .vtpk does not exist, the application automatically switches to use an online map service.

  • While offline, the application can only use a .vtpk.

While creating .vptk files, consider the following:

  • The .vptk packages are ultimately downloaded to the clients, so consider the size of the service area (and thus file size) when creating them to ensure there is adequate memory. There is a balance between detail and performance.

  • The application can use only one .vptk at a time, and a large service area might need to be divided into multiple .vptk areas. In this case:

    • Each .vptk must have a unique name.

    • Each .vptk should cover a specific area in the service territory.

  • A large area can take days to create.

Knowing this, you should decide which areas of your service territory require a .vtpk.


High Precision vs. Low Precision Data Storage

If you have a geodatabase that was created prior to ArcGIS 9.2, the data might be low precision. Replicas cannot be created with low-precision data, and low-precision Geometric Network data must be migrated to high-precision data first. If you attempt to create a replica against low precision data, you receive Error Message 000763.

NOTE: Utility Network geodatabases use high-precision storage by default and no migration is required.

  • To verify the precision of Geometric Network data in ArcCatalog, navigate to the dataset and view its properties. The General tab displays the precision level:

  • If the storage is low precision, there are a few methods to convert to high precision. See the Esri documentation Migrating to High Precision.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.