Configure Tenant Authentication

Portal for ArcGIS is the Schneider Electric and Esri recommended best practice for authentication since it enables secure single sign-on (SSO) access to Portal for ArcGIS-federated feature services. When you request a tenant for an XI series product, Portal for ArcGIS authentication configuration happens through the post-request process.

Setting up authentication using this methodology can vary from organization to organization, depending on their particular needs. One common task, however, is deciding which users will be administrators and which will be viewers, and then grouping the users appropriately. SE needs this information to successfully map your groups to our roles.

IMPORTANT: Integrated Windows Authentication (IWA) with Portal is not a supported method to integrate with your company’s Active Directory (AD). Instead, you must follow the subsequent topics in this chapter to integrate with AD (or any other enterprise identity provider) via a SAML-Compliant Identity Provider.

The distinct advantage of this configuration is that in the event you need built-in users or Active Directory (AD)-based users, usernames and passwords that were set up prior in Portal for ArcGIS can be used to log in to the application.

The topics in this section walk you through tenant provisioning and portal federation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?