Gas Abandon and the Schema.xml

In Designer XI, the gas abandon tool performs an “abandon to attribute field” to accomplish the abandoning procedure. Specifically, the application maps the Designer XI field WorkFunction to the Esri field lifecyclestatus (or the mapped work function field in the Geometric Network), and it uses a coded domain to write to the lifecyclestatus field for gas junctions, gas lines, and gas devices.

As stated in the Prerequisites, Designer XI supports both the Esri Utility and Pipeline Data Model (UPDM) with the Utility Network and also the Geometric Network. If using UPDM with the Utility Network, the appropriate coded domain values for the lifecyclestatus field are provided in the Designer XI Schema.xml by default. You do not need to add them or configure them, and the field mapping is provided out of the box.

everything below this comment is for the internal-only guide and is profiled
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.