File Directories and File Types on Client Machine
This topic discusses the file directory and file types found on the machine where Designer XI is installed.
-
If you installed for the first time prior to the MSIX Migration (roughly June 2022), then the file directory starts with C:\Users\username\AppData\Local or C:\Users\username\AppData\Roaming.
-
If you installed for the first time after the MSIX Migration, then the file directory starts with C:\Users\username\AppData\Local\Packages\ArcFMDesigner_qybjwhg5w8jy8\LocalCache\Local or C:\Users\username\AppData\Local\Packages\ArcFMDesigner_qybjwhg5w8jy8\LocalCache\Roaming.
Install Directory
On the client machine, the install directory and the configuration file name vary based on whether the install date was before or after MSIX migration (see Important note above).
For Designer XI installation prior to the MSIX Migration (roughly June 2022), the install directory is C:\Users\[username]\AppData\Local\DesignerXI. Insert your username in the directory path, replacing [username]. The folder contains installation directories labeled by release number.
|
File |
Description |
|---|---|
|
SE.Geospatial.Electric.DesktopDesigner.exe |
This is the application executable. |
|
SE.Geospatial.Electric.DesktopDesigner.exe.config |
This is a configuration file that includes advanced options |
For Designer XI installation after the MSIX Migration, the install directory is C:\Program Files\WindowsApps\ArcFMDesigner_[version number]_x64__qybjwhg5w8jy8\SE.Geospatial.Electric.DesktopDesigner. Insert the version number of Designer XI on your machine, replacing [version number] in the directory path. Note the difference in the configuration file name.
|
File |
Description |
|---|---|
|
SE.Geospatial.Electric.DesktopDesigner.exe |
This is the application executable. |
|
SE.Geospatial.Electric.DesktopDesigner.dll.config |
This is a configuration file that includes advanced options |

The version number changes when you upgrade Designer XI. The version number can be found using either of the following methods:
-
Windows Settings > Apps > Installed Apps > ArcFM Designer > Advanced Options

-
Designer XI app > User Settings > About > AcrFM Designer XI. In this case the build number is the same as version number.

Client Log File (Designer.log)
On the client machine, the app log file, called Designer.log, is located in C:\Users\username\AppData\Local\Schneider_Electric\Designer or C:\Users\username\AppData\Local\Packages\ArcFMDesigner_qybjwhg5w8jy8\LocalCache\Local\Schneider_Electric\Designer
|
File |
Description |
|---|---|
|
Designer.log |
This is a stream of log output from the Designer XI application. This includes notes on periodic maintenance, initialization notes, records of usages, and error logs. |
AppData Directory
The AppData directory is located in C:\Users\username\AppData\Roaming\SE or C:\Users\username\AppData\Local\Packages\ArcFMDesigner_qybjwhg5w8jy8\LocalCache\Roaming\SE. That directory contains the following folders:
|
Folder |
Description |
|---|---|
|
Catalog |
This contains data downloaded from the Catalog Service. This is information you see in Solution Center > Designer Plugin > Catalog > Equipment for the same tenant. The Catalog Service is defined in Solution Center > Tenancy Plugin > Service Discovery > Catalog field. |
|
DesignerXI |
This contains the offline cache of many auto-generated data files used by the application. For example, it contains eTags (tracking files to determine if the service has updates to download) and feature flags (offline cache of current feature flags enabled for the tenant). |
|
Map Layout |
This contains data downloaded from the Print Service and design print information. It also contains an offline cache of map note graphics. |
|
Styles |
This contains two file types:
|
|
Workflow |
This contains data downloaded from the Catalog Service and dynamic design information. Read more below in the Workflow Directory in AppData section. |
Workflow Directory in AppData
The Workflow directory contains the following files:
|
File |
Description |
|---|---|
|
[designuniqueID].dnx |
This file has a small amount of metadata from the Design and Work Request resources from the Coordination Service. It is primarily the file that contains the “design.” As the design is modified, this file updates to represent the modifications, including all “playback” information required to revert changes and replay navigation choices. It also includes graphics and attributes pulled from the feature service. Finally, it also includes the initial feeder or DesignRegion extract when the work order/design is created. |
|
[designuniqueID].dsr.json |
This is similar to the .dnx file. However, as the design is modified, this file represents only the latest snapshot of the design and includes CU reference information. |
|
[designuniqueID].etag |
This is a tracking file to determine if the service has updates to download. See the topic Entity Tags (eTags) for more information. |
|
CompatibleUnitData.json |
This file contains data downloaded from the Catalog Service. This is information you see in Solution Center > Designer Plugin > Catalog > Compatible Unit for the same tenant. |
|
MacroCompatibleUnitData.json |
This file contains data downloaded from the Catalog Service. This is information you see in Solution Center > Designer Plugin > Catalog > Macro Compatible Unit for the same tenant. |
|
SpecToCuRelationshipData.json |
This file contains data downloaded from the Catalog Service. This is information you see in Solution Center > Designer Plugin > Catalog under Compatible Unit, Macro CU, or Equipment where you have defined a “Relationship” between a CU and Equipment specification. |
Roaming\SE.Geospatial.DesktopDesigner Directory
The Roaming\SE.Geospatial.DesktopDesigner directory contains the following files:
|
File |
Description |
|---|---|
|
DeferUntilOnline.db |
In this directory, the database name appears as DeferUntilOnline_<userId>_<tenantId>.db. This SQLite database stores a queue of commands executed when the user requests a design to be saved. This queue is used regardless of offline/online state and is processed every 1 minute. The following actions currently take advantage of the “defer until online” concept:
|
Logs for Other Services
Logs for on-premises services include:
|
On-Premises Service |
Log Location |
|---|---|
|
Storage Service |
C:\inetpub\wwwroot\DesignStorage\logs |
|
Polyfill Service |
C:\inetpub\wwwroot\AGSPolyfill\logs |