Palettes and Templates

Palettes are collections of Templates. Templates are pre-sketched design components. You can think of Palettes and Groups as folders and sub folders that contain related sets of equipment. They are a way to organize all of your company’s Templates.

Instead of having your designers sketch complicated assets such as switch gears or compressor stations by hand, you can create pre-sketched design components, complete with Attributes, Stamp Graphics, and even Tags. Then, you provide these pre-sketched Templates to your designers. This is a great time saver and also enhances data integrity.

  • You create both Palettes and Templates within the Designer XI application itself.

  • You need the Designer.Admin role in order to create Palettes and Templates.

  • Ensure your Palette and Group exist before sketching a new Template.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.