Install Work Management System Integrations

Earlier in the implementation process, your company and Schneider Electric decided on areas of integration between Designer XI and your Work Management System (WMS). In this step, those integrations are installed on machines at your company site.

IMPORTANT: WMS integration requires administrator permissions.

Configure Backstage Custom Properties

Custom Properties allow designers to save high-level attributes at the Design Level or Work Request Level. These properties are sent along with the Design and Work Request through the workflow, and they can even integrate with your company’s Work Management System (WMS).

See the Solution Center topic Backstage Custom Properties for more information.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.