Fields to Support Display

The Component Information pane displays attributes for selected components.

IMPORTANT: If an attribute is not available or is null, the application does not display it. In other words, while it is generally helpful to map as many of the attributes below as possible to assist the designers, they are not all required for the application to work.

During your specification gathering meeting, team members from your company and your implementation team meet to discuss mapping your equipment specs to the Designer XI application. So, be prepared to provide the location of the following:

Electric

  • Circuit Breaker:

    • Breaking current

    • Gang operated

    • Rated current

    • Type

  • Conductor:

    • Cable resistance (ohms per kilometer)

    • Manufacturer

    • Model

    • Rated current

  • Electric Network Component:

    • Manufacturer

    • Model

    • Type

  • Fuse:

    • Breaking current

    • Rated current

    • Type

  • Guy:

    • Description

    • Name

    • Manufacturer

    • Model

  • Pole:

    • Class

    • Description

    • Height

    • Manufacturer

    • Material

    • Model

  • Riser:

    • Description

    • Height

    • Name

    • Manufacturer

    • Material

    • Model

  • Service Point:

    • Load profile (a category to summarize the average power drawn by the service point)

  • Surface Structure:

    • Height

    • Length

    • Manufacturer

    • Model

    • Type

    • Width

  • Switch:

    • Rated current

  • Transformer:

    • High side connection

    • Low side connection

    • Primary winding rated power

    • Rated kVA

Gas

  • Pipe

    • Diameter

    • Material

  • Valve

    • ValveType

    • Diameter

    • Material

    • NormalPosition

  • Fitting

    • FittingType

    • Diameter

    • Material

  • Meter

    • OperatingPressure

    • Diameter

    • Material

  • GasGenericPointComponent

    • Manufacturer

    • Model

    • Type


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.