Stamp Graphics Properties

The look and feel of the graphic is determined by the various settings in Properties. To modify a graphic, follow these steps:

  1. In the Catalog tab, click once on the graphic to highlight it.

  2. Then, at the bottom of the graphic pane, click Properties.

  3. The Properties are further categorized by Symbol, Layers, and Structure. Each subset of properties controls different aspects of the symbol.

  4. For more information about these Properties, see the Esri help topic Manage Styles.

  5. Always click Apply after making changes. This is the same thing as saving your .stylx file.

  6. Save your Project. Schneider Electric recommends creating and saving a graphics Project. The name of the Project is up to you. This is because you end up re-visiting this Project many times while you are getting your graphics looking just right. Having a dedicated Project saves you time, instead of having to create a new one each time.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.