Supported Symbol Types for Stamp Graphics

Designer XI Stamp Graphics support the following symbol types:

  • Point symbol

  • Line symbol

  • Polygon symbol


Regarding text, the “Text symbol” is not currently supported. However, text can be incorporated into points, lines, and polygons. Incorporating text is explained below in this help topic. Text can also be configured within Map Notes.

Further, the “Dimension Style” is not currently supported. However, dimension lines can be configured within Map Notes.

For more information about Map Notes and their support of text and dimensions, see the Implementation Guide topic Create Map Note Graphics and Publish Service.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?