Configure ArcGIS Server Geometry Service

It is prudent to start setting up Work Management System Integration (WMSI) and the ArcFM Session Manager Function app early in the implementation process. With that in mind, WMSI tools require that the Geometry Service be enabled and shared with the appropriate groups in Portal for ArcGIS. Designer XI relies upon WMSI to locate the feeder nearest a work location of interest. WMSI, in turn, relies upon the ArcGIS Server Geometry Service.

To configure the ArcGIS Server Geometry Service,

  1. Start the Geometry Service

  2. Share the Geometry Service with the groups that were created for the XI Series implementation (for example, all Designer XI groups if implementing Designer XI).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.