Import Existing Templates

You can share Templates across Palettes and Groups by using the Import tool.

To Import Templates, follow these steps:

  1. In the Templates Configuration dialog, click the Group where you want to Import Templates.

  2. Click Import.

  3. Notice an Import Templates dialog appears.

  4. Use the drop-down to choose the other existing Palette that includes the Templates you want.

  5. Expand the Groups that include the Templates you want.

  6. Click Add by each Template you want to include.

  7. If necessary, click the red X to remove a Template.

  8. When finished, click Import.

    NOTE: Do you not see the Import button? Your dialog is likely too small and it is cropping off the button. Expand the size of the dialog.

  9. Click the Save to Cloud button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.